Accessibility Support for FactoryTalk DataMosaix SaaS

This topic describes the accessibility feature in
FactoryTalk DataMosaix SaaS
.
People with visual impairments, or low vision can use
FactoryTalk DataMosaix SaaS
using any screen reader application or web browser extension with a text-to-speech output. Using the screen reader extension or application, users can listen to and interact with the elements on the screen, such as UI labels, messages, and buttons. This makes the
FactoryTalk DataMosaix SaaS
more accessible for people with disabilities and provides a better user experience.
Prerequisites
  • A screen reader extension compatible with your web browser is installed.
  • A screen reader application with a text-to-speech output is installed on your computer.
Using the accessibility feature
After installing the screen reader extension or application, make sure that you have enabled it and it is functional. You can refer to Install a screen reader extension to find the detailed instructions on installing a screen reader extension to the Chrome web browser.
You can start the screen reading functionality by using any of the following methods:
  • Using the mouse pointer:
    • Click any UI label, message, or button on the application you want the system to read out to you.
  • Using the keyboard:
    • Press
      Tab
      to move to the next selectable item and hear the UI label read out.
    • Press
      Enter
      to perform the default action by the selected item or button.
    • Press
      Spacebar
      to open the drop-down list and use the
      Arrow
      to navigate within the list.
The keyboard-only and screen reader users can skip to the main content instead of traversing all the menu items. To perform this:
  1. After the
    FactoryTalk DataMosaix SaaS
    page opens or after the URL refresh, press
    Tab
    using the keyboard.
    The application displays
    Skip to main content
    at the top left corner.
  2. Press
    Enter
    or click
    Skip to main content
    .
NOTE:
Different web browsers have different ways to install and access screen readers. The information provided applies to most web browsers, screen reader applications, and extensions, but you might experience some differences.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal