Setup Data Transformation for CDF
This topic describes the steps to set up and run data transformation where Auth0 is used as Identity Provider (IdP). A user must perform the steps in both,
FactoryTalk DataMosaix SaaS
and Cognite Data Fusion (CDF). CDF, when using Auth0 as the IdP, requires client credentials in order to run data transformations.Provide Feedback