Prerequisites

  • A project is created using
    FactoryTalk DataMosaix SaaS
    .
  • FactoryTalk Alarms and Events Extractor (FTDataMosaix_Alarms and Events_Connector_1.00.00.exe file) must be installed on your system.
    • In extractor file name, 00.00.01 represents the extractor version number and 1092130 indicates the pipeline ID associated with the build that generated the installer. The pipeline ID may vary with each new build.
  • FactoryTalk Alarms and Events must be accessible and ready to establish connection.
  • FactoryTalk DataMosaix SaaS
    users must be associated with Data Configurator role.
NOTE:
FactoryTalk Alarms and Events recommended version >= 6.20.00
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal