Create Project
In
FactoryTalk DataMosaix SaaS
a project is the medium through which members can register applications and extractors for performing data analytics and data visualization. The create project feature is governed by role-based access. You can create project if you are an owner or an administrator of an organization in FactoryTalk Hub
. Once you create a project, you must add members in the organization. Once the members join the organization, you should assign them roles in FactoryTalk DataMosaix SaaS
to use the application. The members can register applications and extractors to ingest and visualize data in FactoryTalk DataMosaix SaaS
.Provide Feedback