Tree View and List View

You can view the assets' structure using the Tree view and List View. You can toggle between the two views by clicking the
Tree View
and
List View
icons.
NOTE:
While in any view, if you want to cancel your current selection and create another asset at root level, you can click the Add Sibling to Top Level icon.
The following is the representation of assets in List View.
Assets - List View
The following is the representation of assets in Tree View
Assets - Tree View
Additionally, the Tree view allows you to perform the Add Asset, Edit Asset, and Delete Asset operation by using the right-click menu.
NOTE:
While in any view, you can use the
Search box
to search an asset. You need to enter few characters to look up the asset. Once the required nodes appear, you can select the desired asset to view the asset details. You can perform operations such as add a child node, edit the asset node, or delete the asset node after searching an asset.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal