Configure Grafana to Connect to FactoryTalk DataMosaix SaaS
Perform the following steps to configure Grafana to connect to
FactoryTalk DataMosaix SaaS
:- Register the application inFactoryTalk DataMosaix SaaS. For information on registering an application inFactoryTalk DataMosaix SaaS, refer to Register Application.
- Download and Install Grafana (available on Chocolaty GUI). Check if the service is running.
- Navigate to localhost:3000 (Default port).
- ProvideUsername:adminandPassword:admin. It is recommended you update the password.
- Install the Cognite Data Fusion plugin.
- Navigate to menu >Administrations>Plugins.
- Search and navigate toCognite Data Fusionand clickInstall.
- Create a new data source in the Cognite Data Fusion portal.
- Navigate to menu >Connections>Connect data.
- Search and navigate toCognite Data Fusion.
- Create a new data source by clickingCreate a Cognite Data Fusion DataSource.
- The data source is created.
Provide Feedback