FactoryTalk DataMosaix SaaS Architecture
FactoryTalk DataMosaix SaaS Architecture

FactoryTalk DataMosaix SaaS
is a SaaS/Cloud application with extractors deployed on the edge that connects to data sources. Applications connect to the FactoryTalk DataMosaix SaaS
cloud to access the data they need. In this document, FactoryTalk DataMosaix SaaS
is both the Rockwell written management console and Cognite Data Fusion (CDF). The Management Console (for example, the app that starts when you click on the FactoryTalk Hub
tile) will be referred to as the FactoryTalk DataMosaix SaaS
Management Console and the greater set of services as FactoryTalk DataMosaix SaaS
. You get to the CDF portion of FactoryTalk DataMosaix SaaS
by clicking on the Main DataMosaix
link in the Management Console.FactoryTalk DataMosaix SaaS
is accessed by logging in to FactoryTalk Hub
. FactoryTalk Hub
is to define users, entitlements, and basic go/no-go access to the application. Fine-grained access is defined inside of the FactoryTalk DataMosaix SaaS
Management Console. This will be covered in detail below. Applications, such as Grafana or PowerBI can be configured to use the data in
FactoryTalk DataMosaix SaaS
. The online documentation covers how to set it up. To read more, refer to Analyze Data.In addition, there are Industry Solutions applications, developed by Rockwell, to suit the needs of specific industries. These are built using
FactoryTalk DataMosaix SaaS
as a foundation. The initial set of applications include FactoryTalk Energy Manager
, Batch Performance Analytics (BPA), and Asset Intelligence (AI) for Mining. From the
Help and Support
section, you can refer to the different forms of FactoryTalk DataMosaix SaaS
help documentation including the getting started information, help topics, and release notes. There are also links that you can use to contact support or view the legal information, license agreement, privacy policy, and more.FactoryTalk DataMosaix SaaS Help and Support

Provide Feedback