Get Support
Support for
) icon in the Management Console and open the
FactoryTalk DataMosaix SaaS
is available via Rockwell product support. To contact the support team, click the Help and Support (Contact Support
menu.Contact Support

The Rockwell support team will answer your question or escalate to Rockwell engineering or Cognite support as required. The direct link to the support team is: https://support.rockwellautomation.com/app/ask/p/6133
Please do not contact the Cognite support team directly.
Provide Feedback