Invalid recipe folder or path
An invalid recipe folder or directory path warning may occur when performing recipe file
operations such as
Export
in the FactoryTalk Batch Recipe Editor
.This error can result if:
- The selected folder is not valid.
- The path to the folder is not valid.
- The selection is not a folder.
Make sure that the folder is valid in File Explorer, and then retry the operation.
Provide Feedback