Diagnostic bar overview
The diagnostic bar provides status information when viewing the
BatchesList
control, PromptsList
control,
and SFC
control in a FactoryTalk View SE
Display Client. 
Item | Description |
|---|---|
![]() | Return to the Home page to view the list of items. |
![]() | View the item count notification for the control type in the display window. If a base filter has been applied, the item count is the number of items after the filter was applied. If there is a syntax error in the base filter, the item count remains unchanged from the unfiltered list. |
![]() | The name of the control type in the display window. |
![]() | The domain and account name information for the logged in user. |
![]() | The status of the FactoryTalk Batch Server's associated data servers and the FactoryTalk Batch Material server. |
![]() | Provides access to the online help |
Provide Feedback