User Preferences dialog box - Views tab
To configure properties that are specific to each view and list in the Network Editor, use the
Views
tab. For all list views, you can enable information tips, alter the behavior of drag and drop, change the appearance of scroll bars, and set selection options. On selected views, you can change the font style and color, as well as the background color.
Provide Feedback