User Preferences dialog box - General tab
The
General
tab is used to configure the basic behavior and appearance of the Network Editor views and dialog boxes. The selections on the General
tab are used in conjunction with other sections of the User Preferences
dialog box.
In the
Options
area, you have the following selections:- Use application colors:Select to assign colors, other than the current Windows colors, to the background and text in the views.
- Use application font:Select to change the font, font style, and size from the default Windows style.
- Information tips:Select to enable single line tips that appear when you move the cursor over a button or field.
- Animate dialogs:Select to have dialog boxes fly out from the location from which they are opened.
- Confirm deletion:Select to display an "Are you sure?" message when you delete an item. Leave disabled to delete an item immediately without confirmation.
- Confirm exit:Select to have the application ask if you want to exit. Leave disabled to exit without a confirmation message.
Provide Feedback