Set the report fonts and colors

There are four areas in a report for which you can edit the fonts and colors:
  • Heading
    – Prints across the top of each page, generally in a larger, bolder font than the rest of the report.
  • Sub Heading
    – Refers to the field names on the report, such as Server. In formatted reports, subheadings print to the left of the actual report data.
  • Body
    – Refers to the actual report data. Body text is usually smaller and lighter than the headings.
  • Footing
    – Prints the page number, date and time that the report is printed across the bottom of each page, generally in a smaller font than the rest of the report.
To set the report fonts and colors:
  1. To change the font type, style, and size of each section in the report template (heading, subheading, body, or footer), select the
    Fonts
    tab.
    FTB_Report_formatted-fonts
  2. Click the button for the report section you want to edit. The
    Font
    dialog box opens.
    FTB_Report_formatted-fonts(select)
  3. Select the desired font, font style/size, and then click
    OK
    .
  4. If your printer supports color printing, you can add color to the report. Select the
    Colors
    tab.
    FTB_Report_formatted-colors
  5. Click the color selection button corresponding to the report section to which you want to add color. The
    Color
    dialog box opens.
  6. Select a color from the
    Color
    dialog box, and then click
    OK
    . You will see a visual representation of each color change in the Report page preview area of the dialog box.
  7. Repeat for the other sections of the report, as desired. When you are finished changing fonts and colors, click
    OK
    to close the
    Report Page Configuration
    dialog box.
  8. Click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal