Edit information tips

Information tips appear when you move the cursor over a button or field. You can change the font and colors of tips, and set tip timing, which determines how soon a tip displays.
To edit information tips
:
  1. Open the
    Network Editor
    .
  2. From the
    View
    menu, select
    User Preferences
    .
  3. On the
    General
    tab in the
    User Preferences
    dialog box, select
    Information tips
    .
  4. Select the
    Tips
    tab.
  5. To enable the
    Background color
    and
    Text color
    lists, disable
    Use Windows colors
    .
  6. To change the tip color, select the text and background colors from the appropriate lists, and then click
    OK
    .
  7. To change the tip font, click the
    Change Font
    button. The
    Font
    dialog box opens. Select the desired font, style, and size from the appropriate list, and then click
    OK
    .
  8. To change the timing of information tips, use the
    Up
    and
    Down
    arrows to change the settings in the Timing area.
    • Delay
      determines how soon a tip displays when the cursor stops on an area with a tip.
    • Visible duration
      determines how long the tip is visible before closing.
  9. Click
    Apply
    .
  10. Click
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal