Report printing formats
The Network Editor report printing feature allows you to print network, server, or result pane information, in a report formatted with headers, footers and column headings (in list reports). There are two report formats available: formatted and list. The header (at the top of the page) consists of the report name, while the footer (at the bottom of the page) contains the printing date/time and the page count.
A formatted report presents the information down the page, with bold field names as shown in this figure.

A list report presents the data in a columnar, spreadsheet format, with one line per data item. The field names become column headings as shown in this figure.

You can customize the reports by setting margins, changing font styles, and selecting text colors. In addition, you can enter custom text that is also included in the footer. (See Set report preferences for more information.)
Provide Feedback