Remove a server
Use the Network Editor to remove a server from your network model.
To remove a server
:- On the mainFactoryTalk Batchserver open theNetwork Editorand navigate to the root network model.
- In theHierarchypane, select the server to remove.
- Click theRemove Serverbutton.
- Click theSynchronizebutton. The servers listed in the model are updated with the new member server list.The server you removed is not updated.
- Log in to the server you removed and open Network Editor.
- Repeat steps 2 through 4 to remove the server manually.
Provide Feedback