FactoryTalk Event Archiver
    The 
FactoryTalk
 Event Archiver’s purpose is to translate the  FactoryTalk Batch
 tab-delimited ASCII electronic batch record files to a user-specified file type. These
        electronic batch record files are maintained separately for each batch created and viewed
        with a word processor or spreadsheet. Many plants have standardized on one of the many
        commercially available Relational Database Management System (RDBMS) software packages. We
        recommend using a high-performance database, such as SQL Server, due to their better
        robustness and performance. The Archiver collects data from each electronic batch record
        file and stores it in the specified RDBMS database format.Provide Feedback