FactoryTalk Batch Server
    The 
 FactoryTalk Batch
 Server is the engine that runs  FactoryTalk Batch
. It is the component that controls system information, phases and recipes. The server
        allows integration with process-connected devices (PCDs) and third-party software packages.
        Prior to opening FactoryTalk Batch View
, the  FactoryTalk Batch
 Server must be running and remain active during all batch functions.The 
 FactoryTalk Batch
 Server operates as a Windows service, which means that the  FactoryTalk Batch
 Server can be configured to start automatically and that control of the  FactoryTalk Batch
 Server can be given to the Windows Service Manager. Because the  FactoryTalk Batch
 Server runs as a service, it does not require an operator to log on to run. Therefore,
        logging on or off Windows during operation does not disrupt the performance of the  FactoryTalk Batch
 Server.Provide Feedback