FactoryTalk Batch Network Editor
    The 
 FactoryTalk Batch
 Network Editor is a utility that indicates where other  FactoryTalk Batch
 and  FactoryTalk Batch
 Material servers are located on the network. This network configuration allows for ease
        of integration with other  FactoryTalk Batch
 components and simplifies the process of reconfiguring a multi-computer system. If  FactoryTalk Batch
        Material Manager
 is also installed the  FactoryTalk Batch
 Network Editor is also used to indicate the location of the material database.Provide Feedback