FactoryTalk Batch Material Manager
     FactoryTalk Batch
        Material Manager
 is used to track material consumption in batch recipes. It consists of two components:
        Material Server and Material Editor.The Material Editor provides an interface to help you create the material database, which
        consists of material, lot, sublot, container, and storage location data. The Material Server
        provides the communication between the material database and the 
 FactoryTalk Batch
 Server. During a batch run, information about available containers is presented to the
        operator for binding decisions. Binding is the process of mapping steps within a control
        recipe to actual equipment in a plant. After a batch is run, quantities consumed or
        distributed are updated in the material database for use in inventory tracking.The Material Server consists of a group of components that work together to service various
        applications. The primary applications that the Material Server services are the Material
        Editor, 
 FactoryTalk Batch
 Server, FactoryTalk Batch Recipe Editor
, and FactoryTalk Batch Equipment Editor
. Any third-party application can also use custom solutions based on the exposed Material
        Object Model (MOM).Provide Feedback