Verify PCD communications
To verify PCD communications:
- SelectStart, point toAllPrograms > Rockwell Software > FactoryTalkBatchSuite>FactoryTalkBatch, and then selectBatchService Manager. TheFactoryTalkBatchServiceManageropens.IMPORTANT: Administratorprivileges are required to perform this procedure.
- Make sureFactoryTalkBatch Serverisselected in theServicebox.
- SelectServer Statistics. TheFactoryTalk Batch ServerStatisticsdialog box opens.
- Select thePCDCommunicationstab. The Data Server Status area displaysthe status of the conversation with the OPC_SIM data server (Phase Simulator), which should be PHASES GOOD, and the INSTRUCTIONBASEDSERVER, which should be INSTRUCTIONS GOOD.

- In theTagVerifyarea, selectStartto begin the verify process. The tag verification process takes several minutes.
- WhentheStatusboxshows COMPLETED, selectOKtoclose the
Provide Feedback