Start FactoryTalk Batch Phase Simulator
FactoryTalk Batch
comes with a phase logic simulation program, referred to as the FactoryTalk Batch
Phase Simulator used to simulate the batch process without connecting to a PCD. The Phase
Simulator imitates the functionality of a data server and can communicate with the FactoryTalk Batch
Server using OPC communication protocol. The Phase Simulator is a powerful tool for
testing, experimentation and demonstration purposes. In this guide, run the sample
demonstration using the Phase Simulator.
TIP:
If the Phase Simulator is required and OPC protocol is used for communications, the
FactoryTalk Batch
Server automatically starts the Phase Simulator. Check the Windows taskbar to see if
the Phase Simulator is started.To run the sample demonstration correctly, open the
ice_cream1.sim
file in the Phase Simulator. To start
FactoryTalk Batch
Phase Simulator:- If the Phase Simulator is already running, maximize it from the Windows taskbar. If the Phase Simulator is not running, selectStart > Rockwell Software >Simulator. TheFactoryTalk BatchPhase Simulator opens.
- SelectIMPORTANT:Administrator privileges are required to perform this procedure.File>Open. TheOpen Simulator Configuration Filedialog box opens.
- From theLook inlist, open theProgram Files > Rockwell Software > Batch > SampleDemo1 > Recipesfolder. Select theice_cream1.simfile, and then selectOpen.
- Minimize thewindow.FactoryTalk BatchPhase Simulator
Provide Feedback