Run the demonstration recipes

To run the demonstration recipes, you must rebuild the recipe directory and verify the recipes in the area model using the
FactoryTalk Batch Recipe Editor
.
IMPORTANT:
Administrator privileges are required to perform this procedure.
To run the demonstration recipes:
  1. Select
    Start > Rockwell Software >
    Recipe Editor
    . The
    FactoryTalk Batch Recipe Editor
    reads the area model.
    TIP:
    If you are logged in with an account that does not have administrator privileges, right-click
    Recipe Editor
    and select
    More > Run as administrator
    to run under elevated privileges.
  2. If prompted, log on to
    FactoryTalk
    . If a message displays asking you to verify the recipes, select
    Cancel
    .
  3. Select
    File
    >
    Rebuild Recipe Directory
    . When the rebuild is complete, select
    OK
    , and then select
    Yes
    to verify the recipes.
  4. When the recipe verification is complete, select
    Accept
    to save the recipes, and then select
    Close
    .
  5. Select
    File
    >
    Exit
    to exit the
    FactoryTalk Batch Recipe Editor
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal