Configuration requirements

There are some constraints in the way the FactoryTalk Batch components can be combined in a FactoryTalk Batch system. For example, you cannot install the Material Manager Server components on the FactoryTalk Batch Server computer, but you can install the Material Client components on the FactoryTalk Batch Server computer. You need to review the configuration constraints and decide on the most appropriate configuration for your purpose.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal