Using a form to edit material properties
- On thePropertiestab, select the record row to edit, and then click theEdit Propertybutton. TheEdit Material Class Propertydialog box opens.

- Modify the material property as desired, and then clickOK.IMPORTANT:If you are changing a value that contains a decimal, use the Delete key to delete the value before typing a new value that contains a decimal. If you type over the old value containing the decimal, the new decimal is not recognized by the application.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog box.TIP:Changing a duplicate property that is assigned to other materials does not affect the other properties.
Provide Feedback