Adding new lots
- From theEdit Materialdialog box, select theLotstab. Existing lots display in ascending order by lot name. You can sort the list by clicking the column header to display an up arrow (ascending) or down arrow (descending).
- Click theNew Lotbutton to insert a new lot record row.
The following is a list of items on theLotstab:ItemDescriptionLot NameUnique name to identify the lot (required).StateCurrent state of the lot (required).QuantityTotal amount of this lot of material (required).Creation DateDate and time the lot was added (view-only).Depletion DateDate and time the lot was deleted (view-only).Controller IDDefaults to the next numeric value in sequence. You can change this to a unique number for PCD phase programming.DescriptionDetailed description of the lot record.RefreshbuttonRe-queries the materials database for lots of this material and repopulates the displayed lot records. - Type the information in the appropriate boxes to define the material lot.
- ClickApplyto save the changes, or clickOKto save the record and close the dialog box.
Provide Feedback