Distributions

If a lot and label are specified in the material requirement for a distribution, the values of the lot and label specification are ignored at unit binding but are assigned to the distributed sublot.
Example
  • MBR_ADD:1 requires an addition of Material_1, Lot_5.
  • MBR_ADD:2 requires an addition of Material_3, Lot_4.
  • MBR_DUMP:1 requires a distribution of Material_6, Lot_1, Label_234.
Unit 1 is selected because it can draw the materials with the specified lots. The lot and label for MBR_DUMP:1 are ignored until the material is distributed to Container_7. The lot and label are then assigned to the material.
FTBMM_GRG_area_model_material
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal