Run an individual phase in auto mode
You may run a phase using AUTO mode in the Equipment view. When a phase is in AUTO mode, P_AUTO displays as the Mode next to the phase icon. While the phase is running, RUNNING is displayed next to the phase icon in dark green text. The information is also displayed in the Phase Specific Information Display area.
- Open the Equipment view.
- Navigate to the Unit in which the desired phase resides. Phases that are not running are in IDLE status.
- Select the phase, and then click theAcquirebutton.
- Click theStartbutton to initiate the phase. TheBatch IDdialog box opens.
- Enter the appropriate Batch ID, and then clickOK.
- The text next to the phase icon lists the current active state and the step index, both in the appropriate color (i.e., RUNNING_1, where RUNNING is the State and 1 is the step index). The mode is displayed as PH_AUTO for operator-controlled Auto mode. The phase transitions to the RUNNINGstate and then to the COMPLETE state after all steps are executed.
- Respond to any prompts in the Instructions view.
- Once the phase is complete it must be reset. Click the appropriate Phase icon, and then click theResetbutton.
- Click theReleasebutton. The Owner is set back to blank, indicating that there is no current owner of the phase.
Provide Feedback