Acquire a phase
To directly command a phase, you must first acquire it. A phase can only be acquired when it is not currently owned.
To acquire a phase:
- Open thePhase Controlwindow.
- Click the button of the phase that you want to acquire.
- Click theAcquire
button, and then confirm the command.TheOprlight for the selected phase turns green. The green indicates that the operator has control of the phase. The mode changes toA.TIP:If the phase you are attempting to acquire is running, the phase is acquired upon completion of that phase.
Provide Feedback