Use the Equipment List view

The Equipment view provides an equipment-centric view of the current batches. The equipment displayed in the Equipment view is defined in the equipment database in the Equipment Editor. There are three levels of equipment which can be viewed within the Equipment view: Area, Process Cell, and Unit. Each level includes run-time data for each equipment resource and up to five custom hyperlinks for each resource. The Area and Process Cell levels also provide a direct link to the Instructions view, which will display all of the instructions for the selected batch. The Unit level provides additional run-time data with respect to the state of the equipment modules.
ePro_EqVwUnitLevel
TIP: If running Internet Explorer version 7.0 or higher, it is possible to have multiple instances of the
eProcedure
Client running in the same browser window. The current user will be logged on to all instances. (See
Running on Internet Explorer version 7.x
and higher for more information.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal