Enable Batch View confirm settings

If you assign specific users and/or groups to a Batch Command or Phase Command and enable the corresponding Confirm policy setting, then only the specified users are allowed to issue the command. (See the
FactoryTalk Batch
Administrator Guide
for more information.)
The
Reactivate
button on the Instructions view is disabled if you do not have permission to reactivate steps. When you access the Instructions view,
FactoryTalk Batch View
checks the
FactoryTalk
Security policy settings for the command. If you have permission to reactivate steps, but the  Step
CONFIRM
value for the ReactivateStep policy setting is
True
, the
Log on to Confirm User
dialog box prompts for a user ID and password when the
Reactivate Step
button is clicked. If the user is authenticated, the step reactivation proceeds. If not, an error message is displayed. (See the
FactoryTalk Batch
Administrator Guide
for more information.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal