About filtering searches using an operator

You can filter search definitions on a column by using an operator (such as Starts With, Contains and so forth) and entering the desired criteria. For example, under the
Timing Properties
, select the
Starts with
operator and then type
every day
to find all searches to be performed daily. You can also filter search definitions on specific column entries (including all or no column entries). For example, in the
Status
column, you could select the operator
Does not contain
and then select the column entry
Disabled
to show only those records that are not disabled.
filtersearches
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal