Items in schedule log cleanup

Once the schedules are created, the information shows in the schedule log cleanup section.
Item
Description
Active
Indicates whether the schedule is active.
If the toggle is turned on, the schedule is active and will run at its next scheduled time. Editing or deleting the schedule is not allowed in this status.
If the toggle is turned off, the schedule is inactive and will run only on demand.
Name
Shows the name of the log cleanup schedule.
Status
Shows the status of the log cleanup schedule.
Schedule Time
Shows the scheduled time for each log cleanup schedule.
Log Type
Shows the log type you specified for each item, which are
Audit, Event
, and
Diagnostics & Health
log.
Criteria
Shows the criteria you specified for each log cleanup schedule.
Action
Shows the actions you can take:
  • start log cleanup schedule: Start the schedule.
  • edit log cleanup schedule: Edit the schedule.
  • delete log cleanup schedule: Delete the schedule.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal