Items in schedule archive cleanup

Once the schedules are created, the information is shown in the schedule archive cleanup section.
Item
Description
Active
Indicates whether the schedule is active.
If the toggle is turned on, the schedule is active and will run at its next scheduled time. Editing or deleting the schedule is not allowed in this status.
If the toggle is turned off, the schedule is inactive and will run only on demand.
Name
Shows the name of the archive cleanup schedule.
Status
Shows the status of the archive cleanup schedule.
Schedule Time
Shows the scheduled time for each archive cleanup schedule.
Criteria
Shows the criteria you specified for each archive cleanup schedule.
Action
Shows the actions that you can take:
  • start archive cleanup schedule: Start the schedule.
  • edit archive cleanup schedule: Edit the schedule.
  • delete archive cleanup schedule: Delete the schedule.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal