Items in Condition - Status dialog
Items in the dialog include:
- OperatorSelect the operator with which to filter the search results:Equal ToorNot Equal To.
- Compare with valueSelect the log record status to which you want to apply the operator:
- Not SetThe default status indicating that no user has set a status for the log record.
- OpenThe issue requires further action.
- ClosedThe issue has been fixed and verified.
- Follow upThe issue has been attended to, but requires additional follow-up.
- DeferredAny action on this issue should be postponed.
- IgnoreDo not attend to this issue.
Provide Feedback