Items in Condition - Severity dialog
Items in the dialog include:
- OperatorSelect the operator with which to filter the search criteria:Equal ToorNot Equal To.
- Compare with valueClick the dropdown arrow to select the severity:
- ErrorAn event published by the system components when an error occurs during system operation, needs attention, and could be critical or fatal.
- WarningAn event published by the system components when something unexpected occurs and needs attention, but is not critical or fatal in nature.
- InformationAn event published by the system components to provide an informational message about the system or tasks.
Provide Feedback