View and include assets in the schedule
You can view the scheduled assets and choose which assets to include in the schedule.
To view and include assets in the schedule
- Do one of the following to select the schedule name for which you want to view and include the assets in:
- OnSchedules, select the schedule name for which you want to view and include the assets in.
- OnSchedules, selectTask properties. The first schedule is selected by default.
- Select the dropdown arrow to view the scheduled assets by location or by asset type.
- Expand the asset tree, and then select the checkboxes next to assets to include them in the schedule. To include all the assets in a container, select the checkbox next to the container.
Provide Feedback