Stop a schedule manually

If you start an inactive Disaster Recovery schedule manually, you can stop it by selecting ftac_web_schedules_stop.
Prerequisites
  • Before stopping a schedule, you must have the
    Edit a schedule
    and
    Command a schedule
    permission to deactivate the schedule.
  • To stop a schedule, you must have the
    Command a schedule
    permission.
To stop a schedule manually
  1. On
    Schedules
    , select the schedule that you want to stop.
  2. In the
    Action
    column, select ftac_web_schedules_stop.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal