Edit schedule properties

When creating a schedule, you configure the settings for the schedule, which can be changed later.
Prerequisite
  • To edit schedule properties, you must have
    Edit a schedule
    and
    Command a schedule
    permission.
To edit schedule properties
  1. On
    Schedules
    , select properties in the upper-right corner. The
    Schedule properties
    page appears.
  2. Select the schedule whose properties you want to edit.
  3. Change the information as needed.
  4. Select
    Save
    to save the modified operation properties or select
    Cancel
    to restore the operation properties to the previous values.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal