Column headings on Schedule
The following table shows the column headings on
Schedules
and their meanings.Column Headings | Descriptions |
|---|---|
Active | Indicates whether the schedule is active. If there is a checkmark in the box, the schedule is active.
|
Status |
|
Name | Shows the schedule name. Schedule names must be unique. |
Schedule Location | Shows the asset for which the schedule is originally created. It could be a scheduled container that includes other assets or an individual asset for which you are creating a schedule. |
Operation | Shows the operation types. |
Description | The description of the schedule definition. This column is not shown by default. To show this column, hover over any column heading, select , and then select to configure the columns to show. |
Last Time |
|
Next Time |
|
Completion Email List |
|
Timing Properties |
|
Action | Starts or stops the schedule. |
Provide Feedback
, and then select
to configure the columns to show.