Activate or deactivate a schedule
Activate a schedule so that it runs automatically at its next scheduled time. A schedule that is being executed as a Run Now event cannot be activated. If the schedule started on its scheduled time, stop the schedule by deactivating it.
Prerequisites
- To run or stop schedules, you must have theCommand a schedulepermission.
- To activate or deactivate schedules, you must have theEdit a scheduleandCommand a schedulepermission.
To activate or deactivate a schedule
- OnSchedules, select a schedule that you want to activate or deactivate.
- In theActivecolumn, turn on the toggle to activate the schedule or turn off the toggle to deactivate the schedule.
Provide Feedback