Column headings on the Event tab
The following table shows the column headings on the
Event
tab and their meanings.Column Headings | Description |
|---|---|
Paper clip icon | Indicates that a file is available. A file attached to the Event Log includes additional information about the event record. You can download the file attachments and find troubleshooting information. |
Logged Time | Shows the date and time that the FactoryTalk AssetCentre database receives a report of the event from the FactoryTalk-enabled software. The Logged Time and Occurred Time might be different if you disconnect from the network while FactoryTalk AssetCentre caches data, or if the time on the server is different from the time on your computer. |
Occurred Time | Shows the date and time that the software records the message. The Logged Time and Occurred Time might be different if you disconnect from the network while FactoryTalk AssetCentre caches data, or if the time on the server is different from the time on your computer. |
Source | Shows the name of the software that logs the event. |
Location | Shows the name of the computer on which the event takes place. |
Severity | The severity of the event:
|
Message | Shows the detailed information about the event such as the type of event, status, the hardware involved, and so forth. A summary of the message appears in the list. The full message appears in the Log Item Details pane. |
Provide Feedback