Column headings on the Audit tab
The following table shows the column headings on the
Audit
tab and their meanings.Column Headings | Description |
|---|---|
Paper clip icon | Indicates that a file is available. A file attached to the Audit Log includes additional information about the event record. You can download the file attachments and find troubleshooting information. |
Logged Time | Shows the date and time when the FactoryTalk AssetCentre database receives a report of the action from the software. The Logged Time and Occurred Time might be different if you disconnect from the network while FactoryTalk AssetCentre caches data, or if the time on the server is different from the time on your computer. |
Occurred Time | Shows the date and time that the software records the action as having occurred. The Logged Time and Occurred Time might be different if you disconnect from the network while FactoryTalk AssetCentre caches data, or if the time on the server is different from the time on your computer. |
Source | Shows the name of the software that logs the action in the Audit Log. |
Location | Shows the name of the computer on which the action takes place. |
Resource | Shows the name of the hardware or software object to which the action happens. For example, the name of the processor that goes online, or the name of the file that is saved. |
Username | Shows the signed-in user who is using the software. It can be a FactoryTalk Security user, a Windows-linked user, or a domain user, depending on how the user logs into the software that generates the audit record. |
Message | Shows the detailed information about the audit such as the type of action, what changes are made, the hardware involved, and so forth. A summary of the message appears in the list. The full message appears in the Log Item Details pane. |
Provide Feedback