Column headings on Report

The following table shows the column headings on Report and their meanings.
Button
Description
Catalog Information
The catalog number of a device.
Device Name
The name of a device. It is hidden by default.
Series
The series of a device.
MAC Address
The MAC address of a device.
Name
The product ID of a device.
Program Name
The name of project created in the controller.
Description
The description of a device. It is hidden by default.
Vendor
The name of the company that offers a device.
Serial Number
The unique serial number of a device.
Warranty Number
The warranty number of a device.
Manufacture Date
The manufacture date of a device.
Lifecycle Status
The lifecycle statues of a device.
Hardware Revision
The hardware revision of a device.
In Device Revision
The existing firmware revision in a device.
Most Current Minor Release
The most current minor firmware revision available for a device.
Most Current Release
The most current major firmware revision available for a device.
Discontinued Date
The announced discontinued date.
Replacement Product
The recommended product to replace the current one.
Replacement Category
The nature of the replacement.
Last Update Date
The last time the lifecycle status was updated.
Product Type
The product type of a device. It is hidden by default.
Product Code
The identification code as defined in the device’s EDS file. It is hidden by default.
Path
The path of a device in the asset tree.
Source File
The name of a RAAI file. The name of the parent node is also shown.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal