Update lifecycle information
Update the lifecycle information of assets in the FactoryTalk AssetCentre server with the Rockwell Automation lifecycle website. For best performance it is recommended to update the lifecycle information when other scheduled tasks are not being performed.
The FactoryTalk AssetCentre Server must have an internet connection to update the lifecycle
information. If the FactoryTalk AssetCentre Server is in your company's intranet and cannot
connect to the PCDC website, then you should configure a forward proxy or your firewall to
permit access.
To update lifecycle information
- OnLifecycle Information, select a container or an individual RAAI file in the asset tree view.TIP:Select the parent container to update lifecycle information for all RAAI files in the parent container.
- SelectUpdate lifecycle information.
- Once the update is complete, the lifecycle information is updated to the FactoryTalk AssetCentre database and the lifecycle status is updated.
Provide Feedback