Refresh lifecycle information
Refresh the lifecycle information of devices on the FactoryTalk AssetCentre client with the FactoryTalk AssetCentre server.
To refresh lifecycle information
- OnLifecycle Information, select a container or an individual RAAI file in the asset tree view.TIP:Select the parent container to update lifecycle information for all RAAI files in the parent container.
- SelectRefresh.
- After the progress, the lifecycle information is updated from the FactoryTalk AssetCentre database to the client and the lifecycle status is updated.
Provide Feedback