View device lifecycle properties

To view the detailed lifecycle information for a single device, you can use the
Properties
pane.
To view device lifecycle properties
  1. On
    Lifecycle Information
    , select a container or an individual RAAI file in the asset tree view.
    TIP:
    Select the parent container to update lifecycle information for all RAAI files in the parent container.
  2. Select
    Report
    .
  3. Select the device row whose properties you want to view.
  4. Select properties in the upper-right corner.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal