Communication protocols
The following table lists the communication protocols that are used for scanning devices.
Protocol | Description |
|---|---|
CIP | Shows the number of devices that are scanned through the Common Industrial Protocol
(CIP). |
SNMP | Shows the number of devices that are scanned through the Simple Network Management
Protocol (SNMP). |
Provide Feedback