D-S
- D -
Diagnostics and Health log
It provides information about the condition of automation devices. For example, a monitoring software product, such as RSNetWorxMD, detects a problem with a device on the automation network. It reports the problem and logs the information in the Diagnostics and Health log.
Disaster Recovery
It ensures quick and accurate file recovery by verifying your devices' program and configuration files against protected master files. The capability provides two types of scheduled operations: Backup and Backup and Compare.
- E -
Event log
It shows database information regarding events that occur in the system. Events are generally system initiated, for example an upload occurred, or a scheduled task completed. Event records are generated by FactoryTalk-enabled products.
- S -
Schedule
It allows you to schedule certain types of operations. The type of operations that can be scheduled are determined by what FactoryTalk capabilities you have purchased.
Search
It allows you to search for and show specified records from one FactoryTalk AssetCentre database source at a time. For example, you could search for events where a specific user performed a task on a specific computer.
Provide Feedback