Column headings on the History tab
The following table shows the column headings on the
History
tab and their meanings.Headings | Descriptions |
|---|---|
Version | The number assigned to a file version. Each file version created begins with the number 1. Each additional version, created by checking in or promoting a file or binder, is assigned a sequential number. |
Time | The date and time that an action was performed on a file or binder. |
Action | The action type that you performed. |
User | The signed-in user who performed the action on a file or binder. |
Comments | Comments entered by the user who performed the action. |
Provide Feedback